FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-L Series > Simultaneous broadcast reception setting for built-in Ethernet port LCPU
FAQ
Simultaneous broadcast reception setting for built-in Ethernet port LCPU
How do I configure the setting to receive simultaneous broadcast during socket communication of L series CPU with built-in Ethernet port?
- Category :
Answer
To receive simultaneous broadcast using UDP, set the parameters as follows.
- Destination IP Address: FF.FF.FF.FFh
- Destination Port No.: Other than FFFFh (Receives the data sent from the specified destination port number.)
: FFFFh (Receives the data sent from all destination port numbers.)
- Destination IP Address: FF.FF.FF.FFh
- Destination Port No.: Other than FFFFh (Receives the data sent from the specified destination port number.)
: FFFFh (Receives the data sent from all destination port numbers.)
- Product Name
- MELSEC-L Series
- Series
- L Series
May I have your opinion?
Related FAQ
- Loop disconnection detection function and heater disconnection detection function of temperature control module
- Conversion speed of L60AD4
- Number of points used for I/O assignment of L26CPU-(P)BT built-in CC-Link function
- Maximum number of connectable modules to LCPU when it is not extended
- FNC connector pin layout in L series I/O module and Q series I/O module