Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22796
  • Release Date : 2018/09/03 17:30
  • Print

How to use LCPU connector terminals

How do I use the LCPU connector terminals (A01 to A20 and B01 to B20)?
Category : 

Answer

The LCPU connector terminals can be used as terminals for built-in I/O function. The setting of the built-in I/O function can be configured with the parameters of the programming tool.
For more details, refer to "MELSEC-L CPU Module User's Manual (Built-In I/O Function)".
Product Name
MELSEC-L Series
Series
CPU

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries