Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22800
  • Release Date : 2018/09/03 17:30
  • Print

Restriction on the use of CPU when branch module and extension module are used

Are there any restrictions on the serial number of LCPU when using the L series branch module and extension module?
Category : 

Answer

Use L series CPU modules whose first 5 digits of the serial number are "13072" or later.
Product Name
MELSEC-L Series
Series
CPU
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?