Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22835
  • Release Date : 2018/09/03 17:30
  • Print

Operation performed when file registers are read

Are file registers read if "Device memory" in the Read from PLC window of GX Developer/GX Works2 is checked? (Standard RAM, created in the following file format)  
Category : 

Answer

Checking "Device Memory" does not read file registers. Switch the Target Memory for "PLC Data" to "Standard RAM" and check "File Register" in the Read from PLC window to read file registers.
Product Name
Engineering Software
Series
Software Package (GPP function)

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries