FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Engineering Software > File export of ladder programs
FAQ
File export of ladder programs
Is it possible to export/import a ladder program created using GX Developer to/from a text file or an Excel-format file in list (mnemonic) representation? Can the operation above also be performed for device comments?
- Category :
Answer
(1) If only GX Developer is used
- The operation cannot be carried out for ladder programs.
- For device comments, copy and paste operations can be carried out with GX Developer and Excel simultaneously opened.
Match the column and row designations of Excel with GX Developer.
(2) If GX Developer and GX Converter (SW[ ]D5C-CNVW) are used
Ladder programs and device comments of GX Developer can be converted into text-format or CSV-format data. Also,
programs and device comments created in text-format or CSV format can be imported into GX Developer.
- The operation cannot be carried out for ladder programs.
- For device comments, copy and paste operations can be carried out with GX Developer and Excel simultaneously opened.
Match the column and row designations of Excel with GX Developer.
(2) If GX Developer and GX Converter (SW[ ]D5C-CNVW) are used
Ladder programs and device comments of GX Developer can be converted into text-format or CSV-format data. Also,
programs and device comments created in text-format or CSV format can be imported into GX Developer.
- Product Name
- Engineering Software
- Series
- Software Package (GPP function)
May I have your opinion?
Related FAQ
- Installing MX Component Version 3 and 4
- I cannot select [Transfer Setup] in GX Developer because it is displayed in gray.
- Compatibility between the Japanese and English versions of GX Developer
- Program by program difference in comments on display
- MX Component Version 4's compatibility with Visual Studio 2010