Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22922
  • Release Date : 2018/09/03 17:30
  • Update : 2018/09/22 16:39
  • Print

Behavior of special relay in offline simulation

In GX Simulator, SM410 is still OFF even after an offline simulation starts.How can I turn ON/OFF SM410?
Category : 

Answer

The constant scan initial value of GX Simulator is 100 ms. Thus, the value of SM410(0.1sec. clock) is OFF in each scan.
To turn ON/OFF SM410, set the constant scan value to other than integral multiples of the clock time.
Set the constant scan setting value in [PLC Parameter] -> [PLC RAS setting] tab.
Product Name
Engineering Software
Series
Software Package (other functions)

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries