Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22943
  • Release Date : 2018/09/03 17:30
  • Print

Setting a high-speed timer and a low-speed timer

I want to set the 100 ms timer for all the 256 points of the parameters of the A2SHCPU. Can I set one type of timer for all the 256 points in GX Developer?
When I use GPPA of Ver. MS-DOS, I can set 0 for the 10 ms timer and can use the 100 ms timer for 256 points of the parameters. Can I use the 100 ms timer for the 256 points in GX Developer?
Category : 

Answer

In the PLC parameter setting of GX Developer, delete the start "200" of the default high-speed timer and input "0". The message indicating that "There is a duplication with the low-speed timer. Do you want to delete the low-speed timer?" is displayed. Click YES.
Product Name
Engineering Software
Series
Software Package (GPP function)

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries