Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22947
  • Release Date : 2018/09/03 17:30
  • Update : 2018/09/25 10:58
  • Print

I cannot open a project file of PX Developer.

When I try to open an fpj file of PX Developer, the message "The drive is unauthorized." is displayed and cannot open the file.
Category : 

Answer

When the total number of characters in the drive/path and project name exceeds 149 one-byte characters (74 two-byte characters), the message "The drive path is unauthorized." is displayed.
Set the drive/path and project name so that the total number of characters of them is 149 one-byte characters (74 two-byte characters) or less.
Product Name
Engineering Software
Series
Software Package (other functions)

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries