FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Network related products > Intelligent Buffer Select of the CC-Link parameter
FAQ
Intelligent Buffer Select of the CC-Link parameter
What do I set for "Intelligent Buffer Select", one of the "Station Information Setting" items of the CC-Link parameter?
- Category :
Answer
Set the size of buffer memory used for transient transmission (by dedicated instructions) to local stations, the standby master station, and intelligent device stations.
For the communication buffer size, specify the size of data to be communicated.
For the automatic update buffer size, specify the necessary size for each intelligent device station.
For the communication buffer size, specify the size of data to be communicated.
For the automatic update buffer size, specify the necessary size for each intelligent device station.
- Product Name
- Network Related Products
- Series
- CC-Link
May I have your opinion?
Related FAQ
- Terminating resistors for RS-485 communication of QJ71C24N
- How to set the numbers of occupied stations for CC-Link local stations
- RS-485 connection between QJ71C24N and an external device
- Difference in specifications between "AJ65BT" and "AJ65SBT" in CC-Link remote I/O modules' model names
- Difference between the CC-Link IE Controller Network and a MELSECNET/H network