FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Network related products > Difference between CC-Link reserved stations and invalid stations
FAQ
Difference between CC-Link reserved stations and invalid stations
What are the differences between a CC-Link reserved station and an invalid station?
- Category :
Answer
- Reserved station
Reserved stations are not actually connected to the network (but will be connected in the future)
but do not appear as data link error stations.
- Invaid station
Invalid stations are stations not detected as data link error stations when powered OFF.
Note that errors cannot be detected.
Reserved stations are not actually connected to the network (but will be connected in the future)
but do not appear as data link error stations.
- Invaid station
Invalid stations are stations not detected as data link error stations when powered OFF.
Note that errors cannot be detected.
- Product Name
- Network Related Products
- Series
- CC-Link
May I have your opinion?
Related FAQ
- Difference in specifications between "AJ65SBTB1" and "AJ65SBTB2" in CC-Link remote I/O modules' model names
- CC-Link slave station's flashing L.ERR LED
- The number of CC-Link modules mountable with a universal model QCPU module
- Clearing data in the QJ71C24N's receiving area buffer memory
- CC-Link master modules' start I/O No. and refresh devices RX/RY