Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22995
  • Release Date : 2018/09/03 17:31
  • Update : 2018/09/25 17:40
  • Print

Settings required for transient transmission

There are multiple MELSECNET/H networks and they each have been connected to a relay station.
Are there any parameter settings required for transient transmission to the CPU module with another network No.?
Category : 

Answer

The routing parameter settings are required for transient transmission to the CPU module with another network No.
The request source station, relay station, and request destination station each requires the settings.

For more details, refer to the following manual.
 - Q Corresponding MELSECNET/H Network System Reference Manual (PLC to PLC network) 7.4.2 Routing function
Product Name
Network Related Products
Series
MELSECNET/H

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries