FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Network related products > Precaution about MELSECNET/H connection (2)
FAQ
Precaution about MELSECNET/H connection (2)
What are the precautions for connecting a Q series redundant system using the MELSECNET/H remote I/O network system?
- Category :
Answer
- Set the network module mounted in system A to station number 0 (multiplexed remote master station).
Set the network module mounted in system B to any station number between 1 and 64.
When the network module mounted in system B is set to station number 0, "LINK PARA. ERROR" occurs.
- For the Network Parameters of both system A and B, set "Network type" to "MNET/H (Multiplexed remote master)".
Also, set the system B's station number as "remote sub-master station".
Set the network module mounted in system B to any station number between 1 and 64.
When the network module mounted in system B is set to station number 0, "LINK PARA. ERROR" occurs.
- For the Network Parameters of both system A and B, set "Network type" to "MNET/H (Multiplexed remote master)".
Also, set the system B's station number as "remote sub-master station".
- Product Name
- Network Related Products
- Series
- MELSECNET/H
May I have your opinion?
Related FAQ
- Precaution about MELSECNET/H connection (1)
- Link data from communication error stations in a CC-Link network
- Mixing line topologies with star topologies in the CC-Link IE Field Network
- Connecting terminating resistors for CC-Link communication
- Refresh timing of bit data and word data in the same CC-Link station