FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Network related products > SB/SW refresh device setting with CC-Link
FAQ
SB/SW refresh device setting with CC-Link
How many points are used when I configure the SB/SW refresh device setting with the parameters of CC-Link?
- Category :
Answer
SB/SW uses 512 points of refresh devices.
- Product Name
- Network Related Products
- Series
- CC-Link
May I have your opinion?
Related FAQ
- Differences between CC-Link IE Control Network and CC-Link IE Field Network
- Assignment for connecting two CC-Link remote input modules (16-point type) (Remote net Ver.1 mode)
- Cause to turn on the ERR LED of a CC-Link master module
- How refresh devices for CC-Link remote inputs and outputs are assigned
- Cascade connections between hubs in the CC-Link IE Field Network