Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 23084
  • Release Date : 2018/09/03 17:31
  • Update : 2018/09/26 13:19
  • Print

FL-net setting of GX Works2

How can I set the parameters of the FL-net interface module with GX Works2?
Category : 

Answer

You can set the parameters of the FL-net interface module with the data operation of the intelligent function module.
For details and operation procedure of the data operation of the intelligent function module, refer to the following manual.

 - GX Works2 Version 1 Operating Manual (Intelligent Function Module)
    2.1 Operations of Intelligent Function Module Data
Product Name
MELSEC-Q Series
Series
FL-net

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries