FAQ
FAQAbout Products
- FAQ > Robots > Industrial/Collaborative Robots-MELFA > Horizontal type robot > Oil is leaking.
FAQ
Oil is leaking.
Oil is leaking from the robot's body.
Answer
Cause:
- Deterioration in the reducer oil seal.
- Too much grease was applied.
- A grease other than the specified grease was applied.
- Excess grease left on the unit when grease was applied.
- Foreign materials have stuck to the oil seal(dust, etc.).
Measures:
- Check the amount of grease that should be applied and the name and product number of the grease.
- Take measures to make sure that dust, etc. does not adhere to joints.
- After applying grease wipe off any grease that is protruding.
- Product Name
- Industrial Robots MELFA
- Series
- FR Series
F Series