Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 23423
  • Release Date : 2018/09/14 15:06
  • Update : 2018/09/26 16:38
  • Print

Compatibility of option units for the GOT1000 series

Answer

The following option units for the GOT1000 series can be used for the GOT2000 series as well.
・ GT15-SOUT
・ GT15-PRN
・ GT15-DIOR
・ GT15-DIO

The following option units for the GOT1000 series cannot be used.
Please replace them with the option units dedicated to the GOT2000 series (GT27***).
・ GT16M-MMR → GT27-MMR-Z
・ GT16M-V4 → GT27-V4-Z
・ GT15V-75V4 → GT27-V4-Z
・ GT16M-R2 → GT27-R2, GT27-R2-Z (*)
・ GT15V-75R1 → GT27-R2, GT27-R2-Z (*)
・ GT16M-V4R1 → GT27-V4R1-Z
・ GT15V-75V4R1 → GT27-V4R1-Z
・ GT16M-ROUT → GT27-ROUT, GT27-ROUT-Z
・ GT15V-75ROUT → GT27-ROUT, GT27-ROUT-Z
(*) The settings for GT27-R2 and GT27-R2-Z differ in the screen design software.

The following option units for the GOT1000 series cannot be used.
Please change the equipment configuration such as adding a USB memory.
・ GT15-CFCD
・ GT15-CFEX-C08SET
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
Option unit
Series
GOT2000 Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries