FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27 > Screen gesture function when the remote personal computer operation function is used
FAQ
Screen gesture function when the remote personal computer operation function is used
Can the screen gesture function on the remote personal computer operation screen when the remote personal computer operation function is used?
Answer
The screen gesture function cannot be used on the remote personal computer operation screen when the remote personal computer operation function is used. The following are the reasons.
1. For the remote personal computer operation function (Serial)
The operation position information is not communicated to the personal computer correctly, and thus a malfunction occurs.
2. For the remote personal computer operation function (Ethernet)
The remote personal computer operation screen is displayed as an overlap window. However, the overlap window is hidden in the screen gesture mode.
1. For the remote personal computer operation function (Serial)
The operation position information is not communicated to the personal computer correctly, and thus a malfunction occurs.
2. For the remote personal computer operation function (Ethernet)
The remote personal computer operation screen is displayed as an overlap window. However, the overlap window is hidden in the screen gesture mode.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (gesture), GOT function (remote personal computer operation)
- Series
- GOT2000 Series