FAQ
FAQAbout Products
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT25 > Remote personal computer operation function (Ethernet)
FAQ
Remote personal computer operation function (Ethernet)
Can the remote personal computer operation function (Ethernet) be used in the GOT2000 series?
Answer
The remote personal computer operation function (Ethernet) can be used in the GOT2000 series as well.
Note the following when using the function.
1. The remote personal computer operation function (Ethernet) license for the GOT2000 Series (GT25-PCRAKEY) is required.
2. For GT Designer3 Version1.185T or later and earlier than Version1.225K,
set "GOT Graphic Ver.1" to the graphics setting. If "GOT Graphic Ver.2" is set,
a message appears saying "This function cannot be used" when GOT calls the
remote personal computer operation function (Ethernet).
Note that "GOT Graphic Ver.2" can be used with GT Designer3 Version1.225K or later.
For the details of the graphics setting, refer to the following manual.
GT Designer3 (GOT2000) Screen Design Manual (SH-081220-AC)
"5.1.5 [Type Setting] dialog ■1 [Basic Setting]"
Note the following when using the function.
1. The remote personal computer operation function (Ethernet) license for the GOT2000 Series (GT25-PCRAKEY) is required.
2. For GT Designer3 Version1.185T or later and earlier than Version1.225K,
set "GOT Graphic Ver.1" to the graphics setting. If "GOT Graphic Ver.2" is set,
a message appears saying "This function cannot be used" when GOT calls the
remote personal computer operation function (Ethernet).
Note that "GOT Graphic Ver.2" can be used with GT Designer3 Version1.225K or later.
For the details of the graphics setting, refer to the following manual.
GT Designer3 (GOT2000) Screen Design Manual (SH-081220-AC)
"5.1.5 [Type Setting] dialog ■1 [Basic Setting]"
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- Supported model (remote personal computer operation function (Ethernet)), license (remote personal computer operation function (Ethernet))
- Series
- GOT2000 Series
May I have your opinion?
Related FAQ
- Compatibility of the option board for the MES interface function
- Changing the bus connection to the Ethernet connection
- Compatibility of the wireless LAN communication unit (GT25-WLAN)
- Connecting FA devices through the wireless LAN communication unit (GT25-WLAN)
- Trial use of the remote personal computer operation function (Ethernet)