FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27 > Compatibility of a commercially available wireless LAN access point
FAQ
Compatibility of a commercially available wireless LAN access point
Can a commercially available wireless LAN access point be used for the wireless LAN connection?
Answer
In the GOT2000 series, a commercially available wireless LAN access point compatible with IEEE802.11b/g/n standards can be used for the wireless LAN connection by using the wireless LAN communication unit (GT25-WLAN).
However, there are the following restrictions.
1. Supported security authentication methods are as follows.
64 bit/128 bit WEP, WPA-PSK (TKIP, AES), WPA2-PSK (TKIP, AES)
2. IEEE802.11n only supports the 2.4 GHz band.
In addition, use WPA-PSK (AES) or WPA2-PSK (AES) for the security authentication method when communicating by IEEE802.11n.
When WEP or TKIP is selected, the wireless LAN communication unit cannot communicate by IEEE802.11n.
The wireless LAN communication unit (GT25-WLAN) can be used as an access point.
* Compatible with GT Designer3 (GOT2000) Version1.144A or later.
Use the BootOS version "C" or later.
* Up to five stations are connectable.
* The standards, which must be complied with by the countries where the unit can be used, differ depending on the hardware version of the wireless LAN communication unit (GT25-WLAN).
For the details, refer to the following Technical News.
・ GOT2000 Series Wireless LAN Communication Unit (GT25-WLAN) Complies with Overseas Radio Laws and Regulations (GOT-A-0096)
However, there are the following restrictions.
1. Supported security authentication methods are as follows.
64 bit/128 bit WEP, WPA-PSK (TKIP, AES), WPA2-PSK (TKIP, AES)
2. IEEE802.11n only supports the 2.4 GHz band.
In addition, use WPA-PSK (AES) or WPA2-PSK (AES) for the security authentication method when communicating by IEEE802.11n.
When WEP or TKIP is selected, the wireless LAN communication unit cannot communicate by IEEE802.11n.
The wireless LAN communication unit (GT25-WLAN) can be used as an access point.
* Compatible with GT Designer3 (GOT2000) Version1.144A or later.
Use the BootOS version "C" or later.
* Up to five stations are connectable.
* The standards, which must be complied with by the countries where the unit can be used, differ depending on the hardware version of the wireless LAN communication unit (GT25-WLAN).
For the details, refer to the following Technical News.
・ GOT2000 Series Wireless LAN Communication Unit (GT25-WLAN) Complies with Overseas Radio Laws and Regulations (GOT-A-0096)
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- Communication unit, peripheral
- Series
- GOT2000 Series