FAQ
FAQAbout Products
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > Ethernet connection with the QnUD(H)CPU
FAQ
Ethernet connection with the QnUD(H)CPU
I want to connect a GOT2000 series model and the QnUD(H)CPU by Ethernet by using QJ71E71-100.
How can I set it?
How can I set it?
- Category :
-
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT25
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT21
Answer
The following describes an example of settings to connect a GT27, GT25, or GT21 model (Ethernet connection model) and the QnUD(H)CPU by Ethernet by using QJ71E71-100.
1. Configure the following settings in GT Designer3 (GOT2000).
◆ For GT Designer3 (GOT2000) Version1.100E or later
(1) Select [Common] → [Controller Setting] → [CH1] from the menu.
Manufacturer: MITSUBISHI ELECTRIC
Controller Type: MELSEC-Q/QS, Q17nD/M/NC/DR, CRnD-700
I/F: Ethernet:Multi
(For GT Designer3 (GOT2000) Version1.170C or earlier, Standard I/F(Ethernet): Multi)
Driver: Ethernet(MITSUBISHI ELECTRIC), Gateway
(For GT Designer3 (GOT2000) Version1.178L or earlier, Ethernet (MELSEC), Q17nNC, CRnD-700, Gateway)
GOT Net No.: 1
GOT Station: 18
(2) Select [Common] → [Controller Setting] → [CH1] → [Ethernet Setting] from the menu.
Host: *
Net No.: 1
Station: 1
Unit Type: QJ71E71/LJ71E71
IP address: 192.168.3.39
Port No.: 5001
Communication: UDP
(3) Select [Common] → [GOT Ethernet Setting] → [GOT IP Address Setting] → [Standard Port] from the menu.
(For GT Designer3 (GOT2000) Version1.170C or earlier, select [Common] → [Controller Setting] → [CH1] → [GOT Standard Ethernet Setting].)
GOT IP address: 192.168.3.18
Subnet Mask: 255.255.255.0
2. Configure the following settings in GX Works2.
(1) Select [Parameter] → [Network Parameter] → [Ethernet/CC IE/MELSECNET] from the menu.
Network Type: Ethernet
Start I/O No.: 0000
Network No.: 1
Station: 1
(2) Select [Parameter] → [Network Parameter] → [Ethernet/CC IE/MELSECNET] → [Action] from the menu.
IP address: 192.168.3.39
For the details, refer to the following.
・ GOT2000 Series Connection Manual (Mitsubishi Electric Products) For GT Works3 Version1 (SH-081197ENG)
"5.3 GOT Side Settings"
"5.4 PLC Side Setting"
1. Configure the following settings in GT Designer3 (GOT2000).
◆ For GT Designer3 (GOT2000) Version1.100E or later
(1) Select [Common] → [Controller Setting] → [CH1] from the menu.
Manufacturer: MITSUBISHI ELECTRIC
Controller Type: MELSEC-Q/QS, Q17nD/M/NC/DR, CRnD-700
I/F: Ethernet:Multi
(For GT Designer3 (GOT2000) Version1.170C or earlier, Standard I/F(Ethernet): Multi)
Driver: Ethernet(MITSUBISHI ELECTRIC), Gateway
(For GT Designer3 (GOT2000) Version1.178L or earlier, Ethernet (MELSEC), Q17nNC, CRnD-700, Gateway)
GOT Net No.: 1
GOT Station: 18
(2) Select [Common] → [Controller Setting] → [CH1] → [Ethernet Setting] from the menu.
Host: *
Net No.: 1
Station: 1
Unit Type: QJ71E71/LJ71E71
IP address: 192.168.3.39
Port No.: 5001
Communication: UDP
(3) Select [Common] → [GOT Ethernet Setting] → [GOT IP Address Setting] → [Standard Port] from the menu.
(For GT Designer3 (GOT2000) Version1.170C or earlier, select [Common] → [Controller Setting] → [CH1] → [GOT Standard Ethernet Setting].)
GOT IP address: 192.168.3.18
Subnet Mask: 255.255.255.0
2. Configure the following settings in GX Works2.
(1) Select [Parameter] → [Network Parameter] → [Ethernet/CC IE/MELSECNET] from the menu.
Network Type: Ethernet
Start I/O No.: 0000
Network No.: 1
Station: 1
(2) Select [Parameter] → [Network Parameter] → [Ethernet/CC IE/MELSECNET] → [Action] from the menu.
IP address: 192.168.3.39
For the details, refer to the following.
・ GOT2000 Series Connection Manual (Mitsubishi Electric Products) For GT Works3 Version1 (SH-081197ENG)
"5.3 GOT Side Settings"
"5.4 PLC Side Setting"
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (communication)
- Series
- GOT2000 Series