FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT25 > Ethernet connection between multiple GOTs and the QnUDVCPU
FAQ
Ethernet connection between multiple GOTs and the QnUDVCPU
How can I set it?
- Category :
-
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT25
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT21
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series > GT37
Answer
The following shows an example of settings to connect multiple GOTs to the built-in Ethernet port of the QnUDVCPU via Ethernet.
1. Configure the following settings in the screen design software.
◆ For GT Designer3 (GOT2000) Version 1:
(1) [Common] → [Controller Setting] → [CH1]
Manufacturer: MITSUBISHI ELECTRIC
Controller Type: MELSEC-Q/QS, Q17nD/M/NC/DR/DSR, CRnD-700
I/F: Ethernet: Multi
Driver: Ethernet(MITSUBISHI ELECTRIC), Gateway
GOT Net No.: 1
GOT Station: 18
(2) [Common] → [Controller Setting] → [CH1] → [Connected Ethernet Controller Setting]
Host: *
Net No.: 1 (virtual)
Station: 1 (virtual)
Unit Type: QnUD(P)V/QnUDE(H)
IP Address: 192.168.3.39
Port No.: 5006
Communication: UDP
(3) [Common] → [GOT Ethernet Setting] → [GOT IP Address Setting] → [Standard Port]
GOT IP Address: 192.168.3.18
Subnet Mask: 255.255.255.0
(4) Configure the settings from (1) to (3) for each GOT by shifting the station number and the GOT IP address.
2. Configure the following settings in GX Works2.
(1) [Parameter] → [PLC parameter] → [Built-in Ethernet]
IP address: 192.168.3.39
(2) [Parameter] → [PLC parameter] → [Built-in Ethernet] → [Open Setting]
Protocol: UDP
Open method: MELSOFT connection (Configure the setting for each GOT.)
For details, refer to the GOT connection manual.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (communication)
- Series
- GOT2000 Series, GOT3000 Series