FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT25 > Ethernet connection between one PLC and two GOTs
FAQ
Ethernet connection between one PLC and two GOTs
Can two GOTs (GOT3000 series and GOT2000 series) be connected to one Mitsubishi Electric PLC via Ethernet?
- Category :
-
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT25
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT21
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series > GT37
Answer
Yes. Multiple GOTs (GOT 3000 series and GOT 2000 series) can be connected to one Mitsubishi Electric PLC via Ethernet. The number of connectable GOTs differs depending on the controller.
1. When connecting to the MELSEC iQ-R series, motion controller CPU (MELSEC iQ-R series), C Controller module (MELSEC iQ-R series), MELSEC-Q, QS, QnA, L, A, or motion controller CPU (Q series)
For Ethernet modules, up to 128 GOTs are connectable (16 or less are recommended).
However, there are the following restrictions.
• For an RJ71EN71, the maximum number of connectable GOTs per network is 119.
• For models other than the RJ71EN71, the maximum number of connectable GOTs per network is 63.
2. When connecting to the MELSEC-FX
When an FX3U-ENET-L is used, up to two GOTs are connectable.
When an FX3U-ENET-ADP is used, up to four GOTs are connectable.
3. When connecting to the Built-in Ethernet port CPU or C Controller module, up to 16 GOTs are connectable.
For the MELSEC iQ-F series, up to 8 GOTs are connectable.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (communication)
- Series
- GOT3000 Series, GOT2000 Series