FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27 > Use of the Ethernet cable
FAQ
Use of the Ethernet cable
Which Ethernet cable can be used for the Ethernet connection between a GOT and a Mitsubishi Electric PLC, a cross cable or straight cable?
- Category :
-
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT25
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT21
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series > GT37
Answer
The Ethernet cable that can be used to connect the GOT and Mitsubishi Electric PLC via Ethernet varies depending on the presence of a hub and the connected devices.
Use the following cables according to the connection configuration.
1. When connecting to the PLC via a hub:
Straight cable
(For an AutoMDI/MDI-X compatible hub, both straight and crossover cables can be used, enabled by the automatic port identification function.)
2. When connecting to the PLC without a hub:
(1) When connecting to the Ethernet module of the PLC
Cross cable
(2) When connecting to the built-in Ethernet port of the PLC
Straight cable or crossover cable
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- Cable
- Series
- GOT2000 Series, GOT3000 Series