Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 23451
  • Release Date : 2018/09/14 15:06
  • Update : 2018/09/26 18:45
  • Print

Port number when using the Ethernet connection

When multiple GOT2000 series models are connected to one PLC by Ethernet, is the GOT communication port number required to be changed?
Category : 

Answer

When multiple GT27, GT25, or GT21 models (Ethernet connection models) are connected to one PLC by Ethernet, the GOT communication port number is not required to be changed.
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (communication)
Series
GOT2000 Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries