FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27 > Enabling/disabling the object gesture function
FAQ
Enabling/disabling the object gesture function
How can I enable/disable the object gesture function?
- Category :
-
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series > GT37
Answer
The object gesture function can be enabled when the following conditions of 1. and 2. are both satisfied.
This function is disable when either 1. or 2. is not satisfied.
◆ GT Designer3 (GOT3000) Version 1
1. Enable the gesture function in the project settings.
Select [Common] → [GOT Type Setting] then select [Use the gesture function].
2. Turn off b0 of Gesture Common Control (GS1794).
Also configure the following settings to enable the object gesture function in the digital image display object. *1
◆ GT Designer3 (GOT3000) Version 1
Select [Object] → [Digital Image Display] then select [Gesture Operation] for [Touch Mode] in the [Digital Image Setting] tab.
*1: This is "Video/RGB display object" for the GT27 model.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (gesture)
- Series
- GOT2000 Series, GOT3000 Series