FAQ
FAQAbout Products
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > Operating the objects with the gesture function using the SoftGOT-GOT link function
FAQ
Operating the objects with the gesture function using the SoftGOT-GOT link function
Can I operate the objects of the GOT with the gesture function using the SoftGOT-GOT link function?
- Category :
-
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GT SoftGOT
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GT SoftGOT > SoftGOT2000
Answer
You cannot operate the objects of the GOT with the gesture function using the SoftGOT-GOT link function, since GT SoftGOT2000 does not support the gesture function.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (gesture), SoftGOT
- Series
- GOT2000 Series, SoftGOT
May I have your opinion?
Related FAQ
- Checking the simultaneous 2-point press switches placed on the screen design software
- Ethernet connection between GT SoftGOT2000 and a PLC
- Using the rugged model in rain
- Operating the screen with the gesture function while using the SoftGOT-GOT link function
- Switching languages on the GOT2000 series