FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27 > Disabling screen gesture mode
FAQ
Disabling screen gesture mode
How can I disable screen gesture mode?
- Category :
-
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series > GT37
Answer
The following actions can disable screen gesture mode.
• Touching the screen gesture mode switch (key code: FF90).
• Touching the full scale display (100% display) switch (key code: FF91).
• Transitioning to the utility screen.
• Switching to the base screen.
• Acquisition of operation rights by the VNC client when the GOT remote access function (VNC server function) is used.
• Loss of operation rights for the GOT network interaction function.
* Place the screen gesture mode switch outside the screen gesture active area.
* For the GOT3000 series, only models with a capacitive-type touch panel are compatible with screen gesture mode.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (gesture)
- Series
- GOT2000 Series, GOT3000 Series