Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 23490
  • Release Date : 2018/09/14 15:06
  • Update : 2018/09/25 17:58
  • Print

PLC access from GX Works2 via the GOT

When connecting a personal computer (GX Works2) and the built-in Ethernet interface of Q03UDECPU via the USB interface of the GOT2000 series, how should I set the connection destination in GX Works2?
Category : 

Answer

When connecting a personal computer (GX Works2) and the built-in Ethernet interface of Q03UDECPU via the USB interface of the GOT2000 series, set the connection destination in GX Works2 as follows.

1. PC side I/F Serial Setting
 ・ Select [USB].

2. PLC side I/F Detailed Setting of GOT
 ・ CPU mode: Select [QCPU (Q mode)].  
 ・ Select [via GOT(Ethernet) transparent mode].
    ・ Model: Select [Ethernet Built-in CPU].
    ・ IP address: Enter the IP address of Q03UDE.

3. Other Station Setting
 ・ Select [No Specification].

Note that the connection is not established unless the following conditions are satisfied.
 ・ Ethernet communication between the GOT and Q03UDE is properly established.
 ・ The connection destination of the transparent function is set to Q03UDE (MELSEC-Q/QS, Q17nD/M/NC/DR, CRnD-700).

For the details, refer to the following.

・ GOT2000 Series Connection Manual (Mitsubishi Electric Products) For GT Works3 Version1 (SH-081197)
 "Chapter 5 ETHERNET CONNECTION"
 "Chapter 23 FA TRANSPARENT FUNCTION"

・ GT Designer3 (GOT2000) Screen Design Manual (SH-081220)
"5.3.6 Setting target channels for the FA transparent function"
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (FA transparent function)
Series
GOT2000 Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries