FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT25 > Use of commercially available SD memory cards for the GOT2000 series
FAQ
Use of commercially available SD memory cards for the GOT2000 series
Can I use commercially available SD memory cards for the GOT2000 series?
- Category :
-
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT25
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT21
Answer
You can use commercially available SD memory cards for the GOT2000 series.
Note that we do not guarantee the operation when commercially available USB memories are used.
For the details, refer to the following Technical News.
Operation Check Results of Non-Mitsubishi SD Cards on GOT2000 Series Units (GOT-A-0065)
Note that we do not guarantee the operation when commercially available USB memories are used.
For the details, refer to the following Technical News.
Operation Check Results of Non-Mitsubishi SD Cards on GOT2000 Series Units (GOT-A-0065)
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- Peripheral (data storage)
- Series
- GOT2000 Series