FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27 > Using with the GOT1000 series in a GOT multi-drop topology
FAQ
Using with the GOT1000 series in a GOT multi-drop topology
Can the GOT1000 series and GOT2000 series be used together in the GOT multi-drop topology?
- Category :
-
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT25
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT21
Answer
The GOT1000 series and GOT2000 series can be used together in the GOT multi-drop topology.
Use GT Designer3 (GOT1000) Version 1.12N or later to write the basic operating system and communication driver to the serial multi-drop connection unit (GT01-RS4-M).
The basic operating system and communication driver cannot be written with GT Designer3 (GOT2000).
Use GT Designer3 (GOT1000) Version 1.12N or later to write the basic operating system and communication driver to the serial multi-drop connection unit (GT01-RS4-M).
The basic operating system and communication driver cannot be written with GT Designer3 (GOT2000).
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (communication), GOT function (multi-drop)
- Series
- GOT2000 Series