FAQ
FAQAbout Products
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT25 > Using the rugged model outdoors
FAQ
Using the rugged model outdoors
Can the rugged model be used outdoors?
Answer
The rugged model can be used outdoors.
Protect the GOT from direct sunlight by attaching a roof or in other ways when using the rugged model outdoors.
Due to direct sunlight, the temperature of the panel surface and inside the control panel may increase. Use the GOT in the environment within the operating ambient temperature range.
Protect the GOT from direct sunlight by attaching a roof or in other ways when using the rugged model outdoors.
Due to direct sunlight, the temperature of the panel surface and inside the control panel may increase. Use the GOT in the environment within the operating ambient temperature range.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- Rugged model
- Series
- GOT2000 Series