Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • No : 23726
  • Release Date : 2018/09/19 17:16
  • Update : 2018/09/20 13:26
  • Print

Combination transformer

Answer

That is described as below.
 
(1) By laying ZCTs for two feeders having different loads, detected by one earth fault directional relay.
     In this case, it is inapplicable.
(2) Because of cables capacity having the same load, two cables are selected and detected by one earth fault directional relay by laying ZCTs respectively.
     In this case, two cables should be passed together to ZCT with a large diameter wherever possible.
Product Name
Protection Relay
Series
MELPRO-A Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries