FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Engineering Software > Types of data backup methods (FX3G series)
FAQ
Types of data backup methods (FX3G series)
What are the differences among the three data backup methods of the FX3G series?
- Category :
-
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series
- FAQ > Controllers > Programmable Controllers MELSEC > Engineering Software
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Main Unit
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Accessories
Answer
1. Data backup using an optional battery
Built-in RAM data and clock data of a programmable controller are held by using an optional battery.
The life of an optional battery is approximately 5 years (ambient temperature: 25ºC ).
For battery replacement guidelines, refer to the User's Manual (Hardware Edition) for the series used.
When an optional battery voltage becomes low, the built-in RAM data and clock data held will be lost.
2. Data backup using an optional memory cassette
Sequence programs are held in the built-in EEPROM of an optional memory cassette.
Maintenance of the built-in EEPROM is not required. However, the number of overwrites is limited. For details, refer to the User's Manual (Hardware Edition) for the programmable controller used.
3. Data backup using the built-in EEPROM of a programmable controller
Latched device data and sequence programs are held in the built-in EEPROM of a programmable controller.
Maintenance of the built-in EEPROM is not required. However, the number of overwrites is limited. For details, refer to the User's Manual (Hardware Edition) for the programmable controller used.
Built-in RAM data and clock data of a programmable controller are held by using an optional battery.
The life of an optional battery is approximately 5 years (ambient temperature: 25ºC ).
For battery replacement guidelines, refer to the User's Manual (Hardware Edition) for the series used.
When an optional battery voltage becomes low, the built-in RAM data and clock data held will be lost.
2. Data backup using an optional memory cassette
Sequence programs are held in the built-in EEPROM of an optional memory cassette.
Maintenance of the built-in EEPROM is not required. However, the number of overwrites is limited. For details, refer to the User's Manual (Hardware Edition) for the programmable controller used.
3. Data backup using the built-in EEPROM of a programmable controller
Latched device data and sequence programs are held in the built-in EEPROM of a programmable controller.
Maintenance of the built-in EEPROM is not required. However, the number of overwrites is limited. For details, refer to the User's Manual (Hardware Edition) for the programmable controller used.
- Product Name
- FX3G, FX3GC
- Product Category
- Main unit, Engineering Software, GX Works2, GX Developer, Accessories, Options
- Series
- MELSEC-F series