FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Engineering Software > FX3U-ENET-ADP connectable programmable controllers in the MELSEC-F series
FAQ
FX3U-ENET-ADP connectable programmable controllers in the MELSEC-F series
Are there any FX3U-ENET-ADP (for Ethernet communications) connectable programmable controllers in the MELSEC-F series?
- Category :
-
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series
- FAQ > Controllers > Programmable Controllers MELSEC > Engineering Software
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Main Unit
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Network/Communication
Answer
The FX3U-ENET-ADP can be connected to the FX3G/FX3GC series (both Ver. 2.00 or later) and the FX3U/3UC series (both Ver. 3.10 or later).
Products which are required for connecting the FX3U-ENET-ADP to the above programmable controllers can be checked using MELSEC-F Series Model selection tool.
* The version of main units can be checked on the "PLC Diagnostics" window of GX Works2 or by monitoring the last three digits of the data in D8001 (PLC type and system version).
* When connecting to the FX3G series, a connector conversion adapter, FX3G-CNV-ADP, is required.
* When connecting to the FX3U series or the FX3UC-32MT-LT(-2), an expansion board, for example, FX3U-CNV-BD, is required.
Products which are required for connecting the FX3U-ENET-ADP to the above programmable controllers can be checked using MELSEC-F Series Model selection tool.
* The version of main units can be checked on the "PLC Diagnostics" window of GX Works2 or by monitoring the last three digits of the data in D8001 (PLC type and system version).
* When connecting to the FX3G series, a connector conversion adapter, FX3G-CNV-ADP, is required.
* When connecting to the FX3U series or the FX3UC-32MT-LT(-2), an expansion board, for example, FX3U-CNV-BD, is required.
- Product Name
- FX3U-ENET-ADP
- Product Category
- Main unit, Engineering Software, Network/Communication GX Developer, GX Works2
- Series
- FX3G, FX3GC, FX3U, FX3UC