FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Connecting local stations to the FX3U-16CCL-M
FAQ
Connecting local stations to the FX3U-16CCL-M
Is it possible to connect local stations to the FX3U-16CCL-M CC-Link master block?
Answer
No, local stations cannot be connected to the FX3U-16CCL-M.
Remote I/O stations, remote device stations, and intelligent device stations can be connected to FX3U-16CCL-M.
Remote I/O stations, remote device stations, and intelligent device stations can be connected to FX3U-16CCL-M.
- Product Name
- FX3U-16CCL-M
- Product Category
- Network/Communication
- Series
- FX3G, FX3GC, FX3U, FX3UC
May I have your opinion?
Related FAQ
- Assignment of remote input device and remote output device of FX3U-16CCL-M
- Communications with a personal computer after the communication parameters for the RS-232C communication equipment are set
- Setting of the FX3U-ENET-ADP Ethernet communication special adapter
- Switching network between 10BASE-T and 100BASE-TX of the FX3U-ENET-L
- Writing a program to a memory cassette