FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Network/Communication > Support of the DHCP (Dynamic Host Configuration Protocol) function by the FX3U-ENET-ADP (for Ethernet communications)
FAQ
Support of the DHCP (Dynamic Host Configuration Protocol) function by the FX3U-ENET-ADP (for Ethernet communications)
Does the FX3U-ENET-ADP support the DHCP function?
Answer
The FX3U-ENET-ADP does not support the DHCP function. Set the fixed IP address using the parameter setting of GX Works2. On GX Works2, select "Parameter" and "PLC Parameter". Click the "Ethernet Port Setting" tab, and set the fixed IP address.
- Product Name
- FX3U-ENET-ADP
- Product Category
- Network/Communication
- Series
- FX3S, FX3G, FX3GC, FX3U, FX3UC