FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Main Unit > Use of latched (battery backed) type auxiliary relay
FAQ
Use of latched (battery backed) type auxiliary relay
The latched (battery backed) type auxiliary relay is not held.
- Category :
Answer
If the OUT instruction using a latched (battery backed) type auxiliary relay number exists in a sequence program, the information held may be overwritten by execution of the OUT instruction. Use the SET instruction instead of the OUT instruction for the device numbers that need to be held.
- Product Name
- FX1S, FX1N, FX1NC, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
- Product Category
- Main Unit
- Series
- MELSEC-F Series
May I have your opinion?
Related FAQ
- Latched (battery backed) area in the data register (D) of the FX3G/FX3GC series
- Models from the FX programmable controllers that support the extended register (R)
- Number of occupied points of special function devices
- Differences in the specifications between the programmable controllers used in Japan and overseas.
- Compliance of the FX programmable controllers with the EU RoHS Directive