Start main contents
Font Size
S
M
L
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC-F Series
>
MELSOFT connection of the FX3U-ENET-A...
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
No : 24903
Release Date : 2019/04/15 11:31
Print
MELSOFT connection of the FX3U-ENET-ADP Ethernet communication special adapter
How many MELSOFT connections of the FX3U-ENET-ADP Ethernet communication special adapter can be open processed simultaneously?
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
Up to 4 connections can be opened.
Product Name
MELSEC-F Series
Product Category
FX3U,FX3UC,FX3G,FX3GC
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
Support of the DHCP (Dynamic Host Con...
MELSOFT connection of the FX3U-ENET-L...
Power supply of the FX3U-ENET-ADP Eth...
AnyWire-compatible master block of th...
Use of latched (battery backed) type ...
page top
HOME
FAQ