FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Positioning Control > Differences in the mounting dimensions and sizes between the pulse output blocks FX2N-1PG and FX3U-1PG
FAQ
Differences in the mounting dimensions and sizes between the pulse output blocks FX2N-1PG and FX3U-1PG
Are there any differences in the mounting dimensions and sizes between the FX2N-1PG and the FX3U-1PG?
Answer
The external and mounting dimensions of the FX2N-1PG and the FX3U-1PG are identical. However, the electrical specifications and connectable FX programmable controllers (FX3U/FX3UC series) are different. For the positioning function, the starting time of the FX3U-1PG became shorter. For details on the positioning function, refer to Appendix C in the FX3U-1PG User's Manual (Manual number: JY997D47301).
- Product Name
- MELSEC-F Series
- Product Category
- FX3U,FX3UC
- Series
- Positioning Control
May I have your opinion?
Related FAQ
- Programmable controller series which the FX3U-1PG pulse output block can be added to
- Positioning blocks/module that can be connected with a manual pulse generator
- Starting time of the FX3U-1PG
- Terminal layout of the FX3U-1PG and FX2N-1PG pulse output blocks
- Output frequency of the FX3U-1PG pulse output block