FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Power supply of the FX3U-ENET-ADP Ethernet communication special adapter
FAQ
Power supply of the FX3U-ENET-ADP Ethernet communication special adapter
Is it necessary to prepare a power supply for driving the FX3U-ENET-ADP separately?
Answer
No, it is not necessary because power is supplied internally from the main unit.
- Product Name
- MELSEC-F Series
- Product Category
- FX3U,FX3UC,FX3G,FX3GC
- Series
- Network/Communication
May I have your opinion?
Related FAQ
- Maximum number of personal computers that can be communicated with the FX3U-ENET-L simultaneously
- Number of remote device stations that can be connected to FX2N-16CCL-M
- Support of the DHCP (Dynamic Host Configuration Protocol) function by the FX3U-ENET-ADP (for Ethernet communications)
- Supported versions of the FX3G/FX3GC series main units for the CC-Link parameter settings of GX Works2
- Accessing the FX3U-ENET-ADP Ethernet communication special adapter at remote locations from GX Works2 via Internet