FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Main Unit > Supported versions of the FX3G/FX3GC series main units for the CC-Link parameter settings of GX Works2
FAQ
Supported versions of the FX3G/FX3GC series main units for the CC-Link parameter settings of GX Works2
Which versions of the FX3G/FX3GC series main units support the CC-Link parameter settings of GX Works2?
- Category :
Answer
Ver2.00 or later is applicable. (GX Works2 with Ver. 1.87R or later is applicable.)
The version of main units can be checked with the last three digits of the data stored in the special register D8001 (PLC type and system version).
(Example) When the special register D8001 is monitored using GX Works2 and the numerical value stored in the D8001 is a decimal number "26200" ,the last three digits "200" represent the version. In this case, the version is Ver.2.00.
The version of main units can be checked with the last three digits of the data stored in the special register D8001 (PLC type and system version).
(Example) When the special register D8001 is monitored using GX Works2 and the numerical value stored in the D8001 is a decimal number "26200" ,the last three digits "200" represent the version. In this case, the version is Ver.2.00.
- Product Name
- MELSEC-F Series
- Product Category
- FX3G,FX3GC
- Series
- Main Unit
May I have your opinion?
Related FAQ
- Overwriting a current value with the high-speed counter comparison instruction
- Using a fixed latched (battery backed) type device as a general type device
- Supported versions of the FX3U/FX3UC series main units for the CC-Link parameter settings using GX Works2
- Maximum number of personal computers that can be communicated with the FX3U-ENET-L simultaneously
- Support of the DHCP (Dynamic Host Configuration Protocol) function by the FX3U-ENET-ADP (for Ethernet communications)