FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > FX series with a built-in USB port
FAQ
FX series with a built-in USB port
Which models of the FX programmable controllers have a built-in USB port?
- Category :
Answer
The FX3S,FX3G/FX3GC series has a built-in USB port.
- Product Name
- MELSEC-F Series
- Product Category
- FX3S, FX3G, FX3GC
- Series
- Main Unit
May I have your opinion?
Related FAQ
- Gratis warranty term of the FX programmable controllers
- Using a fixed latched (battery backed) type device as a general type device
- Positioning blocks/module that can be connected with a manual pulse generator
- Using the FX3U-16CCL-M and FX2N-16CCL-M together
- Connection of the FX3G series and the FX3U-ENET-ADP