FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Positioning Control > Drive products (servo amplifiers) that can be connected to the FX3U-1PG pulse output block
FAQ
Drive products (servo amplifiers) that can be connected to the FX3U-1PG pulse output block
Which drive products can be connected to the FX3U-1PG?
Answer
Servo amplifiers, such as MR-J4-□A and MR-JN-□A, that support pulse train input can be connected.
For connectable drive products, such as servo amplifiers, refer to the example connection in the FX3U-1PG User's Manual (Manual number: JY997D47301).
For connectable drive products, such as servo amplifiers, refer to the example connection in the FX3U-1PG User's Manual (Manual number: JY997D47301).
- Product Name
- MELSEC-F Series
- Product Category
- FX3U,FX3UC
- Series
- Positioning Control
May I have your opinion?
Related FAQ
- Maximum number of personal computers that can be communicated with the FX3U-ENET-L simultaneously
- Differences in the mounting dimensions and sizes between the pulse output blocks FX2N-1PG and FX3U-1PG
- Terminal layout of the FX3U-1PG and FX2N-1PG pulse output blocks
- Target address change during the positioning operation in the FX3U-1PG
- Pulse output system of the FX3U-1PG pulse output block