FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Main Unit > Maximum length of input wiring
FAQ
Maximum length of input wiring
What is the maximum length of input wiring?
- Category :
Answer
Although it depends on the operating environment, wiring within 20 m is generally recommended.
- Product Name
- MELSEC-F Series
- Product Category
- FX1S, FX1N, FX1NC, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
- Series
- Main Unit
May I have your opinion?
Related FAQ
- Number of FX3U-ENET-L Ethernet interface blocks that can be connected to the FX3U series
- Difference between networks called CC-Link and those called MELSEC
- Temperature input modules that can be used with FX3G series
- Number of FX3U-64CCL interface blocks that can be added to a main unit
- FX series with a built-in USB port