FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Main Unit > Supported versions of the FX3G/FX3GC series main units for accessing the other station from CC-Link using the FX3U-16CCL-M CC-Link master block
FAQ
Supported versions of the FX3G/FX3GC series main units for accessing the other station from CC-Link using the FX3U-16CCL-M CC-Link master block
Which versions of the FX3G/FX3GC series main units support the function for accessing the other station from CC-Link using the FX3U-16CCL-M?
Answer
The main units with Ver.2.00 or later can read and write programs of the FX3 series connected to the intelligent device station and can monitor devices.
(GX Works2 with Ver. 1.87R or later is applicable.)
(GX Works2 with Ver. 1.87R or later is applicable.)
- Product Name
- MELSEC-F Series
- Product Category
- FX3G,FX3GC
- Series
- Main Unit, Network/Communication
May I have your opinion?
Related FAQ
- Number of FX3U-ENET-ADP Ethernet communication special adapters that can be connected to the FX3GC series
- Input numbers of the FX programmable controllers
- Station number setting in the "PLC System(2)" tab of PLC Parameter setting on GX Developer when non-protocol communication is performed
- File format that can be saved to a CF card in the FX3U-CF-ADP
- Connection of the FX3GC series and FX3U-ENET-ADP