Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 24954
  • Release Date : 2019/04/18 14:28
  • Print

Using the FX3U-16CCL-M and FX2N-16CCL-M together

Is it possible to add the FX3U-16CCL-M and FX2N-16CCL-M together to one main unit?
Category : 

Answer

No, they cannot be added together. Only one FX3U-16CCL-M can be connected to one main unit. Multiple FX2N-16CCL-Ms can be connected to one main unit (depending on the programmable controller series and the number of other special extension units).
Product Name
MELSEC-F Series
Product Category
FX3G,FX3GC,FX3U,FX3UC
Series
Network/Communication

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries