Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 24965
  • Release Date : 2019/04/23 07:18
  • Print

M8037 (forced STOP signal)

Is it possible to set a programmable controller from RUN to STOP by turning on M8037 in the program of the FX series while the programmable controller is running?
Category : 

Answer

Yes, it is possible. To set the programmable controller to RUN again, while the programmable controller is stopped, set the built-in RUN/STOP switch as follows: RUN → STOP → RUN.
Product Name
MELSEC-F Series
Product Category
FX1S,FX1N,FX1NC,FX3G,FX3GC,FX2N,FX2NC,FX3U,FX3UC
Series
Main Unit

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries