FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Connection of the FX3GC series and FX3U-ENET-ADP
FAQ
Connection of the FX3GC series and FX3U-ENET-ADP
Is optional equipment required for connecting the FX3GC series and FX3U-ENET-ADP?
Answer
Since the FX3U-ENET-ADP can be connected directly to the FX3GC series, optional equipment is not required.
* When the FX3U-ENET-ADP is used with other special adapters, connect the FX3U-ENET-ADP at the last stage (left end).
* When the FX3U-ENET-ADP is used with other special adapters, connect the FX3U-ENET-ADP at the last stage (left end).
- Product Name
- MELSEC-F Series
- Product Category
- FX3GC
- Series
- Main Unit, Network/Communication
May I have your opinion?
Related FAQ
- Supported versions of the FX3G/FX3GC series main units for accessing the other station from CC-Link using the FX3U-16CCL-M CC-Link master block
- Input numbers of the FX programmable controllers
- Supported versions of the FX3U/FX3UC series main units for accessing the other station of CC-Link using the FX3U-16CCL-M CC-Link master block
- How to use built-in high-speed counters
- File format that can be saved to a CF card in the FX3U-CF-ADP