FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Main Unit > Operation of the first special function unit/block in the FX3UC series
FAQ
Operation of the first special function unit/block in the FX3UC series
The first special function unit/block does not operate in the FX3UC series.
- Category :
Answer
Usually, unit number of the first special function unit/block is "K0". However, when the main unit is FX3UC-32MT-LT(-LT2), the unit number "K0" is assigned to the built-in master for CC-Link/LT. Specify "K1" for the unit number of the first special function unit/block.
- Product Name
- MELSEC-F Series
- Product Category
- FX3UC
- Series
- Main Unit
May I have your opinion?
Related FAQ
- Connection of the FX3GC series and FX3U-ENET-ADP
- Supported versions of the FX3G/FX3GC series main units for accessing the other station from CC-Link using the FX3U-16CCL-M CC-Link master block
- Supported versions of the FX3U/FX3UC series main units for accessing the other station of CC-Link using the FX3U-16CCL-M CC-Link master block
- Input of the R device of the FX3U series in the FX-20P
- CC-Link version of FX2N-16CCL-M