FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Engineering Software > Storage media of a project file
FAQ
Storage media of a project file
Is it possible to read a project created in GX Developer from CD-R or CD-RW?
Answer
The project file written in the write-inhibited media, such as FD, CD-R, or CD-RW, cannot be read.
(Condition: The standard Windows status without CD-R/RW writing software)
(Condition: The standard Windows status without CD-R/RW writing software)
- Product Name
- MELSEC-F
- Product Category
- FX1S, FX1N, FX1NC, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
- Series
- Engineering Software, GX Developer
May I have your opinion?
Related FAQ
- Accessories of the FX3UC-16MR/DS-T and the FX3UC-16MR/D-T
- Operation of the first special function unit/block in the FX3UC series
- Reflecting the changes in the communication setting
- Index modifier of bit devices in the FX3G series
- Number of FX3U-16CCL-M CC-Link master blocks that can be connected to the FX3U series